Technical FAQs

Ask a Question

Does the Dynamic Braking IGBT in the ATV58 drives start gating if the run command is present and reference frequency is at 0hz if unit is seeing a line overvoltage condition?

The Dynamic Braking IGBT does not gate unless the main power transistors are also gating. This does not occur until speed reference reaches about 0.2 hz.

CTA-ID : 2017645
Was this helpful?
What can we do to improve the information ?