Technical FAQs

Ask a Question

What type of branch breakers are suitable for use in the EZMT111225, EZMT112225, EZMT113225, EZMT311225, EZMT312225, EZMT313225, EZMT331225, EZMT332225 and EZMT333225?

Issue:
Application

Product Line:
EZM

Cause:
Tenant breaker selection

Resolution:
These EZMT branch units accept the PowerPact QBP-TM, QDP-TM, QGP-TM or QJP-TM tenant circuit breakers.


CTA-ID : 2017822
Was this helpful?
What can we do to improve the information ?