Technical FAQs

Ask a Question

What type of material is the enclosure on the VC*GU made from?<br /><br />* = 1, 2, 3, 4, 5 or 6.

Polycarbonate or plastic.


CTA-ID : 2017460
Was this helpful?
What can we do to improve the information ?