Technical FAQs

Ask a Question

QO220EPD is this Circuit Breaker rated for a 240V Delta heat Trace application?

The QO-EPD Circuit Breaker is rated for 120/240 only, and must be used on a grounded system. It is not rated for application on a straight 240 Vac delta.

CTA-ID : 2017448
Was this helpful?
What can we do to improve the information ?