Technical FAQs

Ask a Question

What are the specifications for the operation of the logic inputs (LI1 - LI4) for the Altivar 11 drive?

Programmable logic inputs
* Power supply + 15 V ( max. 30v)
* Impedance 5 k ohms
* Positive logic: state 0 if <5 V, state 1 if > 11V
* Negative logic: state 1 if < 5V, state 0 if >11 V or  switched off
(A range only)
* Sampling time: 20 ms max



CTA-ID : 2018022
Was this helpful?
What can we do to improve the information ?