Technical FAQs

Ask a Question

What is the speed regulation on the ATV58 unit?

1% of rated motor speed without adjustments or feedback.

+/- 0.1% of rated motor speed with optional analog I/O card and
appropriate tachometer feedback.

+/- 0.02% of rated motor speed with optional digital I/O card and
appropriate encoder feedback.

3% for ATV58HC10N4X-C33N4X


CTA-ID : 2017802
Was this helpful?
What can we do to improve the information ?