Technical FAQs

Ask a Question

Does the ATS48 unit allow kWH power consumption to be monitored via Serial communication?

Yes.

You can monitor KWH in W4074.

In order to use this parameter correctly, it is necessary to configure the exact value of the line voltage ULn via parameter ULN ( W4055 ).


CTA-ID : 2017625
Was this helpful?
What can we do to improve the information ?