Technical FAQs

Ask a Question

What is the replacement Parts for a HOMC42UC load center cover, Series S01

Issue:
Repair parts

Product Line:
QO LC Cover

Cause:
Maintenance

Resolution:
Only the parts listed below are considered to field replacement parts:
Door Hinge - 4028356450K (2 Required)
Door Latch and Spring - 4020284450K
Cover Mounting Screws - 4020513002K (10 screws per kit)
Directory label - LSDL (This is a generic 1-42 circuit label)


CTA-ID : 2017624
Was this helpful?
What can we do to improve the information ?