Technical FAQs

Ask a Question

What is the continuous ampere contact rating for the 9050AO..., 9050HO... pneumatic timers?

They are rated:
Single Pole Single Throw - 15A continuous AC and DC
Double Pole Double Throw - 10A continuous AC and DC


CTA-ID : 2025647
Was this helpful?
What can we do to improve the information ?