Technical FAQs

Ask a Question

Is the 9013 pressure switch a valid part number without the pressure code?

No. You must have the J code pressure setting to order this product. If a list of pressure settings is not available, use J99 and include the set points desired (which must, of course, fall within the range of the pressure switch selected.)

CTA-ID : 2025644
Was this helpful?
What can we do to improve the information ?