Technical FAQs

Ask a Question

Can the Class 8538 Type S combination starters be provided with auxiliary contact(s) on the disconnect means?

Product Line:
 
Type S combination starters
 
Resolution:
 
Yes, use form Y74 for SPDT or Y75 for DPDT. Field installation kits are also available: see Class 9999 accessory section of current digest for selection based on device selected.

Note: This applies to all combination starters regardless of the Class and Type.



CTA-ID : 2025642
Was this helpful?
What can we do to improve the information ?