Technical FAQs

Ask a Question

Does the ATV11 unit have the UFt parameter which allows drive to be set up for multiple and special motors?

No. The motor parameter settings must be changed if the motor is replaced or if another motor is to be connected.

CTA-ID : 2017610
Was this helpful?
What can we do to improve the information ?