Technical FAQs

Ask a Question

What is the catalog number of the actuator which connects the shaft to the handle for a D10 door mounted operator?

The catalog number is 411954.


CTA-ID : 2017436
Was this helpful?
What can we do to improve the information ?