Technical FAQs

Ask a Question

Where should the J70 wire be connected when replacing the filter board on ATV66D33N4U, ATV66D46N4U, ATV66D23M2U, ATV66D33M2U drives because the new one has a J70 wire on it and the old one did not?

There is a capacitor mounted on the existing drive discharge resistor. This should be removed.
The J70 should connect to the top of the discharge resistor. The two wires that were connected to the discharge resistor should be replaced with the top one mounted to the piggyback connector on the J70 connector.


CTA-ID : 2017433
Was this helpful?
What can we do to improve the information ?