Technical FAQs

Ask a Question

Are the 'Feed-thru' lugs on the QO1816M200FTRB rated the same as the main breaker?

Issue:
Product design features

Product Line:
QO Load centers

Environment:
Feed Through lug rating

Cause:
Application

Resolution:
Yes, the feed-thru lugs would be rated the same as the main breaker.


CTA-ID : 2017432
Was this helpful?
What can we do to improve the information ?