Technical FAQs

Ask a Question

Are the Compact NSF breakers ``kiss-free`` when the shunt trip is energized?

The Compact NSF breakers are ``kiss-free`` when the shunt trip is energized. This means that the main contacts will not close even for an instant if a close attempt is made.

CTA-ID : 2017594
Was this helpful?
What can we do to improve the information ?