Technical FAQs

Ask a Question

Can an 8810 2-speed starter be obtained with a High-Low selector switch and a Hand-Off-Auto selector switch?

Yes, use Form C17 for the High-Low switch and Form C for the Hand-Off-Auto switch. These two Forms are added to the catalog number in alphanumeric order. For example, 8810SBG2V02CC17S.


CTA-ID : 2017593
Was this helpful?
What can we do to improve the information ?