Technical FAQs

Ask a Question

What are the functions of the buttons on an 9080GCB circuit protector?

The smaller red button is the on off switch. The larger black and white button is the trip indicator. White shows a tripped status. It is reset by pushing in this button so that only black shows.


CTA-ID : 2017964
Was this helpful?
What can we do to improve the information ?