Technical FAQs

Ask a Question

What is the permissible wire size for the screw clamp terminals on the LR2K____ overload relays ?

For solid or stranded cable: Minimum (1) #18AWG per phase; Maximum (2) #14AWG or (1) #12AWG per phase.


CTA-ID : 2017773
Was this helpful?
What can we do to improve the information ?