Technical FAQs

Ask a Question

Are the Masterpact NT breakers ``kiss-free`` when the shunt trip is energized?

The Masterpact NW and NT frame breakers are ``kiss-free`` when the shunt trip is energized. This means that the main contacts will not close even for an instant if a close attempt is made.
The continuously energized shunt trip blocks the ``Close`` button, preventing any mechanism action at all.



CTA-ID : 2017585
Was this helpful?
What can we do to improve the information ?