Technical FAQs

Ask a Question

What is the largest busplug that can be installed on the AP30210 busway?<br /><br /><br />

Physically, a 600A switch will fit on the busway. It would not be permissible to run more than 225 amps through the busway however.

CTA-ID : 2017405
Was this helpful?
What can we do to improve the information ?