Technical FAQs

Ask a Question

What is the maximum frequency that the Altivar 28 can have the HSP setting set to?

The high speed HSP can go as high as the maximum frequency setting tFr.

tFr can be adjusted in the drC menu up to 400hz and then HSP can be set in the SEt menu.

CTA-ID : 2017894
Was this helpful?
What can we do to improve the information ?