Technical FAQs

Ask a Question

What is the part number for the control wiring terminal strips on the ATV58 unit?

The part # is VZ3N581U. It includes 3 terminal strips.
It has the R1 & R2 relay contact terminal strip.
It contains the I/O points for the Logic inputs and outputs, the relay outputs and the analog inputs for drives with version 4.1 and lower.
It also has the 10 pin connector that includes the analog output for version 5.1 and higher.
It does not include terminals for I/O extension cards.


CTA-ID : 6883
Was this helpful?
What can we do to improve the information ?