Technical FAQs

Ask a Question

What side of the box (or enclosure) is the load center cover (or door) hinged on for an SC2040M200F?

The door is hinged on the Left side, and opens from right-to-left.
This is the same for all of the following catalog numbers:
SC816F200F, SC12L200F, SC2040M125F. SC2040M200F, SC3040M200F & SC3040M225F

CTA-ID : 2017760
Was this helpful?
What can we do to improve the information ?