Technical FAQs

Ask a Question

What is the part number for a wall duct cover plate screw?

Issue:
Maintenance


Product Line:
Wire Management

Environment:
UL, CSA, NEMA/EEMAC Type 1, IEC 60529

Cause:
Replacement hardware due to loss, misplacement.


Resolution:

The part number for a cover plate screw for Class 5250 RWT wall duct is 45102-407-01.


CTA-ID : 2017575
Was this helpful?
What can we do to improve the information ?