Technical FAQs

Ask a Question

What are the dimensions and weight for the 883958E 30-50hp 460v units and 15-25hp 208/230v units NEMA 3R units?

The maximum dimensions for the 30-50hp 460v units and 15-25hp 208/230v NEMA 3R units are:

Height = 52.22 in (1326.39 mm)
Width = 30.32 in (770.13 mm)
Depth = 16.34 in (415.04 mm)

These dimensions include top and side vent hoods.

Weight = 216 lbs (98 kg)




CTA-ID : 2017740
Was this helpful?
What can we do to improve the information ?