Technical FAQs

Ask a Question

What is the ambient temperature operating range for the ATV58 type FVC Flux Vector Drive?

Storage: -25 to +65 C (-13 to +149 F)
Operation:
      Drive controllers ATV58FHU18N4 to U90N4:
-10 to +50 C (+14 to 122 F) without derating
-10 to +60 C (+14 to 140 F) with fan kit and derating of the
current 2.2% per C above 50 C
       Drive controllers ATV58FHD12N4 to D79N4:
-10 to +40 C (+14 to 104 F) without derating
-10 to +50 C (+14 to 122 F) with fan kit and derating of the
current 2.2% per C above 40 C


CTA-ID : 2017715
Was this helpful?
What can we do to improve the information ?