Technical FAQs

Ask a Question

What is the mating cable that fits the ultrasonic XX630A1KAM12

The 2 meter straight micro connector part number is XSZCD101Y. The 2 meter 90 degree micro connector part number is XSZCD111Y.

These are just a few.. for additional selection of cables see Sensors Catalog 9006CT0101 page 526.


CTA-ID : 2017946
Was this helpful?
What can we do to improve the information ?