Technical FAQs

Ask a Question

How does the lever arm attached to the L100 Limit switch.

The splined shaft of the L100 is split, with a set screw threaded into the center of it. The lever arm is held to the shaft by turning the shaft adjustment nut with a allen wrench causing the shaft coupling to expand which holds the lever arm in place.


CTA-ID : 2017936
Was this helpful?
What can we do to improve the information ?