Technical FAQs

Ask a Question

Which transition section is required to add a new EZM 3 phase in 1 phase out metering device to an old EZM 3 phase in 1 phase out metering device?<br />

Use the 3 phase transition for 3 phase in and 1 phase out and also for the 3 phase in and 3 phase out metering devices.


CTA-ID : 2017570
Was this helpful?
What can we do to improve the information ?