Technical FAQs

Ask a Question

Do we have bussed current transformers wih a ratio of 800:1

Issue:
Do we have bussed current transformers wih a ratio of 800:1

Product Line:
Dry type transformers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Our current transformer (CT) offering no longer includes bushing CT`s which were primarily sold to utilities. We now have window ct`s of various sizes with ratios of of 800:5, 5 amps being the standard rating for instruments being used.


CTA-ID : 2017569
Was this helpful?
What can we do to improve the information ?