Technical FAQs

Ask a Question

How can the baud rate for the ATV58 keypad port be reset to 19200 once it has been changed to 9600?

At this point, the keypad will not operate.
Remove line voltage.
Put the 50/60hz switch to the opposite position.
Restore power.
Remove power.
Return the switch back to original location
Return line voltage.
*** NOTE: All drive parameters should be verified. The parameters will have returned to factory default settings. ***

CTA-ID : 2017431
Was this helpful?
What can we do to improve the information ?