Technical FAQs

Ask a Question

What are the dimensional drawings for the ATV58 top mounted fan kits?

Go to website and download the instruction bulletin for these products.  The document number is 8806DB0004

Height of ventilation fan kit :
VW3A58821: 16mm (0.63 in)
VW3A58822: 25mm (1.00 in)
VW3A58823: 25mm (1.00 in)
VW3A58824: 25mm (1.00 in)
VW3A58825: 60mm (2.36 in)
VW3A58826: 60mm (2.36 in)

CTA-ID : 2017413
Was this helpful?
What can we do to improve the information ?