Technical FAQs

Ask a Question

Is a 1/2 inch NPT conduit adapter available for the XVE Indicating Banks?

Use the XVBC00 conduit adapter since the diameter of the holes on the XVEC Indicating Banks and XVBC Indicating Banks are the same.


CTA-ID : 2037322
Was this helpful?
What can we do to improve the information ?