Technical FAQs

Ask a Question

On an EconoFlex KD46 drive what is the voltage reading between J-27 and J-28?

These 2 pins are the feeds for the fans which are 12 vdc.

These are located on the power board and it is the same for all the size units.

CTA-ID : 2017930
Was this helpful?
What can we do to improve the information ?