Technical FAQs

Ask a Question

Can the 8501 KP or KPD`s be used for switching DC?<br /><br />

The type 8501KP and KPD relay contacts are rated up to 28 VDC for 10 A resistive loads.


CTA-ID : 2017924
Was this helpful?
What can we do to improve the information ?