Technical FAQs

Ask a Question

What is the mating cable that fits the ultrasonic XX512A1KAM8 sensor?

The 2 meter straight nano connector part number is XSZCS141. The 2 meter 90 degree nano connector part number is XSZCS151.

These are just a few.. For additional selection of cables see Sensors Catalog 9006CT0101 page 520 thru 524.

CTA-ID : 2017922
Was this helpful?
What can we do to improve the information ?