Technical FAQs

Ask a Question

Can a SC2040M200C be applied on a system rated 22Kaic?

The SC2030M200C is rated for use on a system rated 10Kaic maximum. It cannot be modified for a high short circuit rating.


CTA-ID : 2017913
Was this helpful?
What can we do to improve the information ?