Technical FAQs

Ask a Question

What size speed potentiometer is recommended for the Altivar ATV58?

The drive has a 10 VDC power supply rated for 10 mA.
The AI1 analog input has an impedance of 30 k Ohms
This will accept any potentiometer from 1k to 10k Ohms.


CTA-ID : 6815
Was this helpful?
What can we do to improve the information ?