Technical FAQs

Ask a Question

Can the trip rating of the EZM31600CB main breaker be changed to a lower amperage rating?

Issue:
Product design Features

Product Line:
EZM Metering

Environment:
Ampere ratings

Cause:
Application

Resolution:
The EZM31600CB is obsolete and has been replaced by the EZM31600GCBC(65k AIC) or EZM31600JCBC(100k AIC) devices. Below are the ONLY trip Rating Columns available for the Old EZM31600CB. 

The following catalog numbers are the 3 pole rating column kits:
600 amp is PA3600RC (OBSOLETE, NLA with NO REPLACEMENT)
700 amp is PA3700RC
800 amp is PA3800RC (OBSOLETE, NLA, with no REPLACEMENT)
1000 amp is PA31000RC (OBSOLETE, NLA with no REPLACEMENT)
1200 amp is PA31200RC
1600 amp is PA31600RC


CTA-ID : 2017896
Was this helpful?
What can we do to improve the information ?