Technical FAQs

Ask a Question

What is the catalog number for the closing plate to be used when the start stop pushbutton kit 8911DPB1 is removed from an 8911DPSG starter?

Use the 9999SG3 NEMA 1 enclosure closing plate.

CTA-ID : 2017892
Was this helpful?
What can we do to improve the information ?