Technical FAQs

Ask a Question

What is the catalog number for a plug-on, 225 ampere, sub-feed lug kit for a Single Phase ONLY QO load center?

Issue:
Product design features

Product Line:
QO Load centers

Environment:
load center accessories

Cause:
Application

Resolution:
The 225amp sub-feed lug kit part number is QO2225SL and can ONLY be used in the Square D, QO SINGLE PHASE, load centers, Series G1 (see Note #1), S1 or S2, rated 150 - 225 ampere.
NOTE #1: Use only in Series G1 single phase load centers manufactured since 8/8/1986 (date code H08Sxxxx). The date code is stamped on the wiring diagram or box label. Also, the Interior Label located on the load centers interior assembly will list Type QOC breakers.
NOTE #2: DO NOT USE in any Square D QO 3-phase load center, 300 - 400 ampere QON load center or other manufacturers load centers or panelboards. Please refer to the Installation Bulletin supplied with the device for further restrictions regarding mounting these devices or adjacent branch circuit breakers.


CTA-ID : 2017880
Was this helpful?
What can we do to improve the information ?