Technical FAQs

Ask a Question

What is the part number for the fan in the Size 6 Altivar 66 drive such as ATV66C10N4U, ATV66C13N4U, ATV66C15N4U or ATV66C19N4U?<br />

First, identify if the drive is a Design A, B or C.
This unit had a design change in 1998 and subsequently some parts changed.
The design A unit was manufactured up until end of May 1998. These controllers DO NOT have a ``1`` as the seventh digit of the serial #.
The Heatsink fan (larger fan on bottom of unit) part # for Design A is VZ3V666
The stirring fan part # for Design A is VZ3V667

The Design B & C Do have a ``1`` as the seventh digit of the serial #.
The Heatsink fan part # for Design B & C is VZ3V670
The stirring fan part # for Design B & C is VZ3V671

The serial # is located beside the nameplate sticker on the top Right hand side of unit --the serial # is on a smaller white sticker with bar code


CTA-ID : 2009849
Was this helpful?
What can we do to improve the information ?