Technical FAQs

Ask a Question

What is the AIC rating of the EJB type branch breakers used in the NF panels?

Issue:
What is the AIC rating of the EJB type branch breakers used in the NF panels?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The EJB breaker has an AIR of 65 kA at 480Y/277 Vac.


CTA-ID : 2017545
Was this helpful?
What can we do to improve the information ?