Technical FAQs

Ask a Question

Do we make a E stop turn to release in 30mm for use in an hospital MRI magnetic resonance imaging room?

Our push button operators and control stations are not recommended for use in hospital MRI rooms due to the metal components such as springs and contacts which can interfere with the MRI equipment.

CTA-ID : 2017543
Was this helpful?
What can we do to improve the information ?