Technical FAQs

Ask a Question

What is the temperature range of the 9050JCK timers?

-18 degrees F (-28 degrees C) to + 131 degrees F (+55 degrees C) operating and -67 degrees F (-55 degrees C) to + 185 degrees F (+85 degrees C) storage for the JCK11 through 59.

- 10 degrees F ( -23 degrees C) to + 130 degrees F (+54 degrees C) operating for the JCK 60 and 70.


CTA-ID : 2017542
Was this helpful?
What can we do to improve the information ?