Technical FAQs

Ask a Question

What is the resistance for the 8910DPA 9998DA1, 9998DA2 and 9998DA3 coils in 120V and 208V versions?<br />

Issue:
What is the resistance for the 8910DPA 9998DA1, 9998DA2 and 9998DA3 coils in 120V and 208V versions?


Product Line:
Definite Purpose Contactors

Environment:
Products sold and used in the United States

Cause:
Resistance information needed for the 8910 contactors

Resolution:
All values are +/- 10% at 40 degrees C:

9998DA1 at 120V is 199.3 Ohms; at 208V is 735.0 Ohms
9998DA2 at 120V is 90.1 Ohms; at 208V is 302.0 Ohms
9998DA3 at 120V is 16.7 Ohms, at 208V is 52.2 Ohms


CTA-ID : 2017797
Was this helpful?
What can we do to improve the information ?