Technical FAQs

Ask a Question

What does the display show on a ATV58 drive if the Auto Restart is set, and the drive faults?

The Auto restart allows an automatic restart of the drive controller if the cause of the fault has disappeared and a run command is maintained. This is only possible for the following faults: OSF, ObF, OtF, LFF, OLF, OPF, OHF, SLF, EPF, CnF.

The fault will be displayed on the keypad for the amount of time set in paramter tAr (menu 6). These faults will be included in the fault history. The number of restarts is controlled by parameter nAr ( menu 6).

CTA-ID : 2017871
Was this helpful?
What can we do to improve the information ?