Technical FAQs

Ask a Question

Does the SC3040M200F accept tandem or quad branch breakers?

Issue:
Product design features

Product Line:
Combination Service Entrance Devices

Environment
Branch breakers

Cause:
application

Resolution:

The load center distribution section of the SC3040M200F accepts Homeline branch breakers and the interior is a 30 space - 40 circuit interior. The interior will accept up to 10 HOMT tandem or 4 HOMT quad branch breakers.


CTA-ID : 2035253
Was this helpful?
What can we do to improve the information ?