Technical FAQs

Ask a Question

What is the line voltage tolerance for the LH4N?

The LH4N line voltage tolerance is -15% to +10% on all values for respective voltages.

208...240 (LH4-N1**LU7)
380...415 (LH4-N1**QN7)
440...480 (LH4-N1**RT7)
208...240 (LH4-N2**LU7)
380...415 (LH4-N2**QN7)
440...480 (LH4-N2**RT7)
208...690 (...N230LY7 to ...N285LY7)


CTA-ID : 2017404
Was this helpful?
What can we do to improve the information ?